Define general device properties
Define general device properties on
Device Definition
.To define general device properties:
- OnController Organizer, double-click the device to openModule Properties.
- OnModule Properties, selectOverview.
- OnOverview, selectDevice Definition.
- Complete the parameters and selectOK.
Provide Feedback