Diagnose a problem with a device
Use
Device Information Diagnostics
to diagnose a problem. Diagnostics is disabled when:
- You are operating offline.
- An Identity mismatch exists (for simplex devices).
- An Identity mismatch exists on both Module A and Module B (for duplex devices).
To diagnose a problem with a device:
- OnController Organizer, double-click the device to openModule Properties.
- OnModule Properties, selectDevice Information.
- OnDevice Information, selectDiagnostics.
- (Optional) If automatic refresh for some parameters stops, selectRetry.
- OnDevice Information Diagnostics, view device diagnostics.
Provide Feedback