Node Output Tags
This table shows the node output tags. These tags apply to Bulletin 440S GuardLink-enabled taps, Bulletin 440G GuardLink-enabled switches, 440E GuardLink-enabled LifeLine 5, and 440N GuardLink-enabled door lock switches. When a non-guard locking device connects to a tap, the connected device ignores the lock and unlock commands. All devices can execute the ResetDevice.
Tag Name | Automatic Diagnostic | Data Type | Description |
|---|---|---|---|
Lock | No | BOOL | 0 = Cancels the previous lock command for the client device (does not unlock the device) 1 = On the transition from 0 to 1, sends a lock command to the client device |
Unlock | No | BOOL | 0 = Cancels the previous unlock command for the client device (does not lock the device) 1 = On the transition from 0 to 1, sends an unlock command to the client device |
ResetDevice | No | BOOL | 0 = Cancels the previous ResetDevice command for the client device 1 = On the transition from 0 to 1, sends a power cycle reset command to the client device. Use this command to clear a fault in the client device. |
Provide Feedback