Interface Output Tags

This table shows the descriptions of the output tags for the 432ES-IG3 network interface device.
Tag Name
Automatic Diagnostic
Data Type
Description
Ch0
No
CHANNEL_GL:O:0
Ch0.LockUnlockEn
No
BOOL
0 = Lock/Unlock command is disabled
1 = Lock/Unlock command is enabled
0 is the default.
Ch1
No
CHANNEL_GL:O:0
Ch2
No
CHANNEL_GL:O:0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal