Port Configuration view

Use the
Port Configuration
view to configure the basic port settings of the devices connected to the switch. These settings determine how data is received and sent between the switch and the attached device. Use this view to:
  • Enable the port.
  • Select if you want the port and the device to auto-negotiate the link speed and duplex mode.
  • Select the port speed and duplex mode.
TIP: The port can only be configured when the device is online. Most data is only displayed when the device is online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal