Enable data transmission on change of state

Enable data transmission when an input point changes state.
To enable data transmission on change of state
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, select the checkbox for each input point to enable change of state for the
    Off -> On
    (LOW to HIGH) and the
    On -> Off
    (HIGH to LOW) transition.
    • Select = The input device produces data cyclically at the Requested Packet Interval (RPI) and immediately upon change of state for the selected point.
    • Clear = The input device produces data cyclically at the RPI for the selected point.
      TIP:
      Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal