Enable diagnostic latching

Configure each point on the device to latch diagnostic members so that they remain set after they are triggered.
Prerequisites
  • Make sure that the connection is configured for Data.
To enable diagnostic latching
  1. On the tab for the device, select
    Configuration
    .
  2. In the
    Points
    view, in the
    Enable Diagnostics
    Latching
    column, enable or disable diagnostic latching by selecting or clearing the checkbox, respectively, for the selected point.
    TIP:
    Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal