Enable data transmission on change of state

Enable data transmission when an input point changes state from the
Off -> On
(LOW to HIGH) and the
On -> Off
(HIGH to LOW) transition. When this feature is enabled, the input device produces data cyclically at the Requested Packet Interval (RPI) and immediately upon change of state for the selected point. If this feature is not enabled for a point, the input device only produces data cyclically at the RPI for that point.
Prerequisites
  • Make sure that the connection is configured for Data.
To enable data transmission on change of state
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, in the
    Enable Change of State
    column, select the checkbox for each input point on which you want to enable change of state data transmission.
    TIP:
    Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal