PWM Cycle Limit value is over range

The Cycle Limit value is greater than the maximum of 127. Enter a value from 1 through 127 and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal