Points Input Filter Time Off->On or On->Off value is under range
The Points Input Filter Time Off->On or On->Off value is less than the minimum of 0. Enter a value from 0 through 30000 and apply the changes.
Provide Feedback