Counter Input Filter Time Off->On or On->Off value is over range
The Counter Input Filter Time Off->On or On->Off value is greater than the maximum of 30000. Enter a value from 0 through 30000 and apply the changes.
Provide Feedback