Device-defined output tags (integer)

The set of tags associated with a device depends on the device type and the communication format. For each operational mode, integer or floating point, there are three sets of tags:
  • Input
  • Output
  • Configuration
This table includes the output tags for 1756 analog output devices operating in integer mode.
Member Name (as listed in Tag Editor)
Data Type
Description
Ch0Data
INT
The channel output value in counts where the minimum producible output is -32,768 counts, and the maximum producible output is 32,767.
Ch0DataEcho
INT
The current channel output value in counts where the minimum producible output is -32,768 counts, and the maximum producible output is 32,767.
OutGroupFault
BOOL
Indicates if a channel fault has occurred on any output channel.
Ch0InHold
BOOL
Indicates if the output channel is currently holding until the output value is sent to the device (O data type, Ch0Data member) matches the current output value (I data type, CH0Data member) within 0.1% of the channel’s full scale.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal