Device-defined configuration tags (integer)

The set of tags associated with a device depends on the device type and the communication format. For each operational mode, integer or floating point, there are three sets of tags:
  • Input
  • Output
  • Configuration
This table includes the configuration tags for the 1756 analog input devices operating in integer mode.
Member Name (as listed in Tag Editor)
Data Type
Description
RealTimeSample
INT
Real Time Sample
- Determines how often the input signal is to be sampled in terms of milliseconds.
ModuleFilter
SINT
Module Filte
r - Configures the module filter value for all channels on the module and provides superior frequency filtering at the selected value and its harmonics.
  • 0 = 10 Hz
  • 1 = 50 Hz
  • 2 = 60 Hz
  • 3 = 100 Hz
  • 4 = 250 Hz
  • 5 = 1,000 Hz
Ch0RangeType
SINT
Range Type
- Configures the channel’s input range which determines the signal range the input channel can detect. Input range values are:
  • 0 = -10 to 10V
  • 1 = 0 to 5V
  • 2 = 0 to 10V
  • 3 = 0 to 20 mA
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal