Alarms view parameters

The parameters in this view
appears shaded under these conditions:
  • Run mode
  • Project Safety Secured mode
  • Point Mode
    =
    Not Used
Parameter
Description
Enable High High and Low Low Alarms
Enables or disables the High High and Low Low process alarms for the individual channel by selecting or clearing the checkbox.
High High
Sets the High High alarm trigger point. Valid values are from -32768 through 32767. The default is 32767.
The
High High
value must be equal to or greater than the
High
value.
Low Low
Sets the Low Low alarm trigger point. Valid values are from -32768 through 32767. The default is 0.
The
Low Low
value must be equal to or less than the
Low
value.
High High and Low Low Deadband
Specifies the value where a High High or Low Low alarm, once set, will not disable as long as the input value remains within the deadband range of the alarm trigger point. The deadband prevents the alarm from cycling on and off if the process value hover near the alarm threshold.
Valid values are from 0 through 32767. The default is 0.
Enable High and Low Alarms
Enables or disables the High and Low process alarms for the individual channel by selecting or clearing the checkbox.
High
Sets the High alarm trigger point. Valid values are from -32768 through 32767. The default is 32767.
The
High
value must be greater than the
Low
value.
Low
Sets the Low alarm trigger point. Valid values are from -32768 through 32767. The default is 0.
The
Low
value must be greater than the
Low Low
value.
High and Low Deadband
Specifies the value where a High or Low alarm, once set, will not disable as long as the input value remains within the deadband range of the alarm trigger point. The deadband prevents the alarm from cycling on and off if the process value hover near the alarm threshold.
Valid values are from 0 through 32767. The default is 0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal