Points view parameters

Parameter
Description
Point
Indicates the point to which the configuration applies.
Fault Delay
Specifies the fault delay limit from 0 ms through 255 ms. The default is 80 ms.
This parameter is not available in Run and Remote Run modes.
Data Direction
Specifies the direction of the data. Valid values for each channel are:
  • Input/Output
    (default)
  • Input
  • Output
This parameter is not available in Run and Remote Run modes.
Enable Web Server
Enables the web server.
This parameter is not available in Run and Remote Run modes.
Enable Output Group Power Fault Reporting
Enables reporting of power faults.
This parameter is not available in Run and Remote Run modes.
Enable Output Group Fault
Enables output group fault when actuator power supply is unavailable.
This parameter is not available in Run and Remote Run modes.
Enable Digital Out Auto Restart
Enables the device to auto restart a digital output.
This parameter is not available in Run and Remote Run modes.
TIP:
If all the following conditions are met, selecting
Apply
or
OK
automatically sends the information to the controller. The controller then tries to send the information to the device if the device's connection is not inhibited.
  • You are online in Program, Remote Program, or Remote Run mode.
  • This controller is the owner controller.
  • You have changed the device's configuration in the software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal