Limits view parameters
Parameter | Description |
|---|---|
High Clamp | Specifies the desired high clamp limit value from -32768 through
32767. The default value for current and voltage is 32767. The High Clamp value must be greater than the
Low Clamp value.This parameter is not available in Run mode and when the
Disable All Alarms checkbox is selected. |
Low Clamp | Specifies the desired low clamp limit value from -32768 through
32767. The default value for current and voltage is -32768. The Low Clamp value must be less than the
High Clamp value.This parameter is not available in Run mode and when the
Disable All Alarms checkbox is selected. |
Unlatch | Unlatches only the corresponding alarm named to the left of the
Unlatch button.This parameter is only available when online. |
Parameter | Description |
|---|---|
Diable All Alarms | Disables all process alarms. Disabling all alarms also disables other features in the
Limits view. Unlatch All and
Unlatch remain enabled.This parameter is not available in Run mode. |
Latch Limit Alarms | Latches all limit alarms. This parameter is not available in Run mode and when the
Disable All Alarms checkbox is selected. |
Unlatch All | Unlatches all the process alarms. This parameter is only available when online. |
Provide Feedback