Fault/Program Action view parameters

Parameter
Description
Channel
Indicates the channel to which the configuration applies.
Communication Fault Mode
Specifies the channel's output behavior when the communication between controller and output device is broken. Valid values are:
  • Hold Last State
  • Go to Low Clamp
    (default)
  • Go to High Clamp
  • Use Fault Value
This parameter is not available in Run mode.
Communication Fault Value
Specifies the fault value from -32768 through 32767. The default is 0.
This parameter is available when
Communication Fault Mode
is set to
Use Fault Value
. It is not available in Run mode.
Program Mode
Specifies the channel's output behavior when in Program mode. Valid values are:
  • Hold Last State
  • Go to Low Clamp
    (default)
  • Go to High Clamp
  • Use Program Value
This parameter is not available in Run mode.
Program Value
Specifies the program value from -32768 through 32767. The default is 0.
This parameter is available when
Program Mode
is set to
Use Program Value
. It is not available in Run mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal