Channels view parameters (output devices)
Parameter | Description |
|---|---|
Channel | Indicates the channel to which the configuration applies. |
Output Range | Specifies the output range. Valid values are:
This parameter is not available in Run mode. |
High Engineering | Specifies the scaling high units from -32768 through 32767. The
default is 10000. This parameter is not available in Run mode. |
Low Engineering | Specifies the scaling low units from -32768 through 32767. The
default is 0. This parameter is not available in Run mode. |
Provide Feedback