Channels view parameters (input devices)
Parameter | Description |
|---|---|
Channel | Indicates the channel to which the configuration applies. |
Input Range | Specifies the input range. Valid values are:
This parameter is not available in Run mode. |
Digital Filter | Specifies the digital filter value from 0 ms through 10000 ms. The
default is 0 ms. This parameter is not available in Run mode. |
High Engineering | Specifies the scaling high units from -32768 through 32767. The
default is 16383. This parameter is not available in Run mode. |
Low Engineering | Specifies the scaling low units from -32768 through 32767. The
default is 3277. This parameter is not available in Run mode. |
Real Time Sample (RTS) | Specifies the real time sample value from 1 ms through 5000 ms. The
default is 100 ms. This parameter is not available in Run mode. |
Provide Feedback