CJ Calibration view parameters (thermocouple devices)

Parameter
Description
Channel
Indicates the channel to which the configuration applies.
Calibration Range
(Thermocouple, CJ)
Indicates the calibration range as
0 ohm to 12.9K ohms
.
Calibration Status
Indicates the status of the calibration per channel as the calibration occurs. Valid values include:
  • OK
  • Error
Start Calibration
Starts the calibration process while online.
This parameter is not available in Run mode and Remote Run mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal