Calibration view parameters (thermocouple devices)
Parameter | Description |
|---|---|
Channel | Indicates the channel to which the configuration applies. |
Calibration Range (Thermocouple, Input) | Indicates the calibration range as 0 mV to 78.125
mV . |
Calibration Status | Indicates the status of the calibration per channel as the
calibration occurs. Valid values include:
|
Start Calibration | Starts the calibration process while online. This parameter is not available in Run mode and Remote Run mode. |
Provide Feedback