Calibration view parameters (input devices)

Parameter
Description
Channel
Indicates the channel to which the configuration applies.
Calibration Range
(Voltage and Current)
Indicates the calibration range as follows:
  • 0V to 10V
  • -10V to 10V
    (0V must be applied for low scale)
  • 0V to 5V
  • -5V to 5V
    (0V must be applied for low scale)
  • 0 mA to 20 mA
  • 4 mA to 20 mA
    (default)
Calibration Status
Indicates the status of the calibration per channel as the calibration occurs. Valid values include:
  • OK
  • Error
Start Calibration
Starts the calibration process while online.
This parameter is not available in Run mode and Remote Run mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal