Device-defined data types (output devices)
Device-defined data type names vary for each device depending on selections made when the device was created.
These tables include information for these data types:
- input (as indicated by an "I")
- output (as indicated by an "O")
- configuration (as indicated by a "C")
Device-defined data type: AB:1718_19_DOn:C:0
Connection Type: Data
Member Name | Type | Style | Valid Values |
|---|---|---|---|
Pt0x.FaultMode | BOOL | Decimal | 0 = Transition to user-defined value 1 = Hold Last State |
Pt0x.FaultValue | BOOL | Decimal | 0 = Output is off 1 = Output is on |
Pt0x.ProgMode | BOOL | Decimal | 0 = Transition to user-defined value 1 = Hold Last State |
Pt0x.ProgValue | BOOL | Decimal | 0 = Output is off 1 = Output is on |
Pt0x.FaultFinalState | BOOL | Decimal | 0 = Output is off 1 = Output is on |
Pt0x.ProgramToFaultEn | BOOL | Decimal | 0 = Channel remains in Program mode 1 = Channel remains in Fault mode |
Pt0x.DiagEn | BOOL | Decimal | 0 = Diagnostics are disabled 1 = Diagnostics are enabled |
Pt0x.FaultValueStateDuration | SINT | Decimal | 0 = Forever 1 = 1 second 2 = 2 seconds 5 = 5 seconds 10 = 10 seconds |
Device-defined data type: AB:1718_19_DOn:I:0
Connection Type: Data
Member Name | Type | Style | Valid Values |
|---|---|---|---|
RunMode | BOOL | Decimal | 0 = Idle 1 = Run |
ConnectionFaulted | BOOL | Decimal | 0 = A connection exists between the device and the controller 1 = Bad |
DiagnosticActive | BOOL | Decimal | 0 = No diagnostics active 1 = One or more diagnostics are active or the prognostics threshold is reached |
DiagnosticSequenceCount | SINT | Decimal | -128...127 The value of 0 is skipped except during device power-up. |
Pt0x.Data | BOOL | Decimal | 0 = Off 1 = On |
Pt0x.Fault | BOOL | Decimal | 0 = A fault does not exist 1 = A fault exists |
Pt0x.Uncertain | BOOL | Decimal | 0 = Data is valid 1 = Validity of data is uncertain. Device is operating outside its designed operating range, or data is under manual or override control. |
Pt0x.NoLoad | BOOL | Decimal | 0 = No Load condition does not exist 1 = No Load condition exists, meaning a signal wire is disconnected from the channel or the RTB. |
Pt0x.ShortCircuit | BOOL | Decimal | 0 = Short Circuit or Overcurrent condition does not exist 1 = Short Circuit or Overcurrent condition exists |
Device-defined data type: AB:1718_1719_DOn:O:0
Connection Type: Data
Member Name | Type | Style | Valid Values |
|---|---|---|---|
Pt0n.Data | BOOL | Decimal | 0 = Off 1 = On |
Provide Feedback