HART Command view
Use the
HART Command
view to automatically configure the HART Field Device with user supplied PV Damping
and Range
values.When these features are enabled, the device sends the
PV Damping
and PV Range
values to the HART Field Device connected to the channel.Provide Feedback