Channels view parameters (HART Output)
The
Channels
view includes these parameters:Parameter | Description |
|---|---|
Channel | Shows the channel number to which this configuration applies. |
Output Range | Determines the output range for the Current output. |
Enable HART | Enables HART functionality on the channel. |
Output State During Program Mode | Determines channel action when the controller transitions to Program mode.
|
Output State During Fault Mode | Determines channel action when a fault occurs.
|
High Signal | Sets one of the four constants in the scaling equation. High Signal is in terms of the input signal units and corresponds to High Engineering when scaled.High Signal must be greater than Low Signal . |
Low Signal | Sets one of the four constants in the scaling equation. Low Signal is in terms of the input signal units and corresponds to Low Engineering when scaled. |
Units (Signal) | Shows the unit of measurement for High Signal and Low Signal . |
High Engineering | Sets one of the four constants in the scaling equation. High Engineering corresponds to High Signal and helps determine the engineering units that the signal values scale into. |
Low Engineering | Sets one of the four constants in the scaling equation. Low Engineering corresponds to Low Signal and helps determine the engineering units that the signal values scale into. |
Units (Engineering) | Shows the unit of measurement for High Engineering and Low Engineering and for the channel’s input value. |
Enable Diagnostics | Enables short circuit and open wire detection on the channel when selected. |
Provide Feedback