Channels view parameters (RTD)

The
Channels
view includes these parameters:
Parameter
Description
Channel
Shows the channel number to which this configuration applies.
Sensor Type and Range
Shows the sensor type and expected measuring range for the channel.
This parameter is set in the
Ch0x
view.
Number of Wires
Shows whether the sensor to be used has a 2-wire, 3-wire or 4-wire configuration.
This parameter is set in the
Ch0x
view.
Wire Resistance
Shows the wire resistance value for a 2-wire sensor. The value can be between 0 and 5000 ohms (input in 1/100 ohm) and is set in the
Ch0x
view.
High Signal
Sets one of the four constants in the scaling equation.
High Signal
is in terms of the input signal units and corresponds to
High Engineering
when scaled.
High Signal
must be greater than
Low Signal
.
Low Signal
Sets one of the four constants in the scaling equation.
Low Signal
is in terms of the input signal units and corresponds to
Low Engineering
when scaled.
Units (Signal)
Shows the unit of measurement for
High Signal
and
Low Signal
.
High Engineering
Sets one of the four constants in the scaling equation.
High Engineering
corresponds to
High Signal
and helps determine the engineering units that the signal values scale into.
Low Engineering
Sets one of the four constants in the scaling equation.
Low Engineering
corresponds to
Low Signal
and helps determine the engineering units that the signal values scale into.
Units (Engineering)
Shows the unit of measurement for
High Engineering
and
Low Engineering
and for the channel’s input value.
Digital Filter
Sets the time constant for a first order lag filter used to smooth noise transients on the input with a range from 0 through 32767. When set to 0, no filtering takes place.
Disable Alarms
Determines whether process alarms are generated.
  • If selected, the device does not generate process alarms.
  • If cleared, the device generates process alarms.
Enable Diagnostics
Enables short circuit and open wire detection on the channel when selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal