Alarms view parameters

The
Alarms
view includes these parameters:
Parameter
Description
Disable All Alarms
Prevents the device from generating any of the four process alarms (LL, L, H, and HH) or the rate alarm and does not allow access to any of the alarm configuration properties.
High High Limit
Sets the trigger point in Engineering Units. HHAlarm is set to 1 when the input signal moves above this limit.
High Limit
Sets the trigger point in Engineering Units. HAlarm is set to 1 when the input signal moves above this limit.
Low Limit
Sets the trigger point in Engineering Units. LAlarm is set to 1 when the input signal moves below this limit. The Low Alarm Limit must be greater than or equal to the Low Low Limit and less than the High Limit.
Low Low Limit
Sets the trigger point in Engineering Units. LLAlarm is set to 1 when the input signal moves below this limit. The Low Low Limit must be less than or equal to the Low Limit.
Deadband
Allows the process alarm status bits to remain set, even if the alarm condition disappears, as long as the channel data remains within plus or minus the deadband value of the process alarm. This
Deadband
value is entered in engineering units.
Rate Alarm Limit
Sets if the rate of change between input samples on this channel exceeds the rate specified in this field in Engineering Units.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal