Diagnose a problem

Diagnose these problems from the
Points
view:
  • Whether a short circuit fault exists.
  • Whether a no load fault exists.
To diagnose a problem with an output point
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, in the
    Diagnostics
    column for the point, click the diagnostics button.
  3. In
    Ptxx Diagnostics
    , view the diagnostics for the point.
See also
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal