Diagnose a problem with a point
Use
Ptxx Diagnostics
to view the diagnostics information for an individual point.To diagnose a problem with a point
Diagnostics
is disabled when:- You are operating offline.
- An identity mismatch exists.
- On the tab for the device, selectPoints.
- In thePointsview, in theDiagnosticscolumn for the point, click the diagnostics button.
- InPtxx Diagnostics, view the diagnostics for the point.
See Also
Provide Feedback