Configuration Errors
If an invalid Configuration is sent to the module, a connection error will occur. Also, when a module has multiple "owners", both controllers must have the same Configuration data for the module. Refer to the section on "Configuration", above, for further explanation and error codes.
Provide Feedback