Documentation
The primary sources for detailed information about this module are the Spectrum Controls document, "0300330-01_A0(Manual_5069_OV16F_SC)", referred to throughout this document as the "User’s Manual", and sometimes called an "Operations Manual".
Available for download from the "SC website" and/or the Studio 5000 Help options are:
- User’s Manual, AOP, Datasheet
- "Owner’s Guide", Technical Notes, Revision Notes, FAQ,
- Presentations, Application stories,
- Sample Projects, EDS files, Firmware Updates, etc.,
- RA Logix Control Systems Recommended Literature Reference Document IASIMP-RM001J-EN-P which can be downloaded from the Studio 5000 Help:Online Books option.
Also refer to RA publication "Compact 5000 I/O Digital Modules documentation, PN 5069-UM004", available for download at the Rockwell Automation website (www.rockwellautomation.com).
Also in this section:
Provide Feedback