Communication

5069 Backplane Communication
  • Connected producer/consumer multicast IO communication.
  • Settable RPI (0.2 to 750.0 ms).
  • Support for multiple controllers using "Listen Only".
  • Local chassis operation, or Remote chassis operation (over CIP network).
  • Unconnected messaging from controller (MSG instruction) or from a CIP network client. Typical uses include Reset or Reconfigure the module.
NOTE:
Refer to detailed protocols and MSG examples described in the module’s "User’s Manual.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal