Alarm Configuration

Use this tab to configure the Spectrum Controls 1734sc-IE2/4CH HART analog module channel alarms.
On this tab, you can:
  • select the channel you want to configure
  • set process alarms
  • choose to disable all alarms
  • enable the latch rate alarm
  • enter rate alarms
  • unlatch alarms for selected channel
Tip
: The module’s configuration information is stored in the controller and the controller configures the module.
Note
: The 1734sc-IE2/4CH Owner’s Guide, which is available online by following the hyperlink on the Vendor tab, provides additional configuration information for some of the parameters discussed in this help file.
Channel
Click one of the channel buttons to display its information on this tab.
Disable All Alarms checkbox
Check this box to disable all alarms for a channel.
Latch Rate Alarm checkbox
When you enable this alarm, a Rate Alarm indication will remain set even when the alarm condition goes away. This latch allows you to maintain the alarm even after the condition ceases. The alarm will only unlatch with an explicit message acknowledging the alarm (unlatch service).
UnLatch Alarm Button
When you select the Unlatch button, all portions of the alarms for the current channel will unlatch as the result of an explicit message (unlatch service request) sent to the module.
Process Alarms
High High Alarm
Set the level of input to a channel that will cause the module to set the High High alarm. The alarm will remain until the input returns below this level, unless it is within the deadband, or as long as the alarm is latched.
High Alarm
Set the level of input to a channel that will cause the module to trigger the High alarm. The alarm will remain until the input returns below this level, unless it is within the deadband, or as long as the alarm is latched.
Low Alarm
Set the level of input on a channel that will cause the module to enable the low alarm. The alarm will remain until the input returns above this level, unless it is within the deadband, or as long as the alarm is latched.
Low Low Alarm
Set the level of input to a channel that will cause the module to indicate a low low alarm. The alarm remains until input returns above this level, unless it is within the deadband, or as long as the alarm is latched.
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
If:
  • you are online in Program, Remote Program or Remote Run mode and,
  • this controller is the owner controller and,
  • you have changed the module’s configuration in the software, when you click the Apply or the OK button, the information is automatically sent to the controller. The controller tries to send the information to the module (if the module’s connection is not inhibited). If you don’t click Apply, your changes are not sent to the controller.
Help
Click this button for help on this tab.
Related Topics
  • Reconfigure an I/O Module Programmatically - refer to RSLogix5000 HELP
  • Reset Latched Status on an Analog Module - refer to RSLogix5000 HELP
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal