Support
Website
Online support is available at the Spectrum Controls website (the "SC website”) at www.spectrumcontrols.com. (hotlink from AOP Vendor tab). See also "Documentation” section above.
Contacts
A list of distributors is available on the "SC website”. Rockwell Automation currently provides telephone technical support for certain Spectrum Controls products. Questions about the 1756sc-IFH8, its Add-on-Profile, or its Sample Projects, should be referred to Technical Support at:
|
|
For other locations, check the www.rockwellautomation.com/support website for Rockwell Automation Customer Support phone numbers. The support "Knowledgebase” at this website may contain information about known issues for this module. Prior to calling for technical assistance, please review the "Owner’s Guide”, Chapter 9, "Testing Your Module.”
Versions and FW Updates
The latest firmware version is 1.17 (as of August 2022). A release history is available from the "SC website”. All FW versions since release are compatible with this Add-on-Profile.
This module contains Flash memory which allows field upgrades to the module firmware to be performed by the user. Refer to the "Owner’s Guide” for details. Firmware update kits can be downloaded from the "SC website”.
Module Replacement
This module supports RIUP (Removal and Insertion Under Power) from chassis while chassis power is applied. Reconfiguration of the module is not needed when replacing a module. Configuration data is retained in the controller and is sent to the module when the IO connection is established.
NOTE
: Refer to the "Owner’s Guide” for proper procedures and Safety recommendations for RIUP. Arcing could cause an explosion in a hazardous location installation. Performing RIUP while the field-side is powered requires EXTREME CAUTION. Unintended machine motion or loss of process control can occur.
NOTE
: Proper handling precautions must be used to avoid damage to electronic components from Electrostatic Discharge. Refer to the "Owner’s Guide” for proper procedures.Procedures and policies for returning a product to Spectrum Controls for service are available in the "Owner’s Guide” and on the "SC website”. Your local distributor may also be able to provide information or assistance. Refer to the website for a list of distributors.
Provide Feedback