Parameters View

The Parameters view allows the user to view and edit Ethernet Actuator parameters.
TIP: Information on the Parameters view is only available when the project is online and the device is connected to the network.

Parameter Groups

The parameters that are displayed in the table are filtered by Parameter Groups. The group of parameters that is displayed is selected using the Parameter Group Filter drop-down menu.

Parameter Table Controls

The controls used to read, edit and write the device parameters are described in the table below.
Parameter Table Controls
Refresh symbol
Refresh Table
Reads the current parameter values from the device and updates the table.
Pencil symbol
Edit Parameter
Edit the selected parameter value. This will display the Parameter Edit dialog to allow the user to modify the parameter value. If the changes made in the edit dialog are accepted, the new parameter value is written to the device.
TIP: This button is disabled for read-only parameters.
Magnifying glass symbol
View Bitstring Details
Display the bitstring details for the selected parameter. This will display the Parameter Details dialog with bit status and description information.
TIP: This button is only enabled for parameters with bitstring values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal