Troubleshooting
NOTE
: Before attempting to maintain or troubleshoot a unit, read the detailed information and IMPORTANT
safety recommendations in the "SLP85xD User Manual" available at this link: SLP85xD High-Precision Weigh Modules - Documentation .Module Indicators/LEDs
Refer to the section on "Indicators and LEDs".
Module Reset
The module can be RESET from the button in the AOP's Module Info Page, or by cycling power to the device.
RSLogix5000/Studio5000 Diagnostics
RSLogix5000 and Studio5000 software indicates module fault conditions in the following three ways:
- Warning signal on the main screen next to the module, when the IO connection is broken.
- Fault message in a screen's status line, with notification in the Tag Editor. General module faults are also reported in the Tag Editor. Diagnostic faults are only reported in the Tag Editor.
- Status on the Module Info Page
Refer to the "SLP85xD User Manual" for detailed information on status, diagnostics, error codes, and alarms.
Provide Feedback