General
This "Basic Module Information" (BMI) provides quick access to a list of the main module functions, some attributes, and the location of more detailed module information.
NOTE
: When developing an application, or troubleshooting a significant problem, it is IMPORTANT to read and follow more detailed module information, including safety recommendations.
The primary source of detailed module information is the manual, "IND570 Terminal PLC Interface Manual" available from the IND570 Documentation CD (P/N # 30205330) included with the terminal. This is referred to as the "manual" in this BMI.NOTE: In this BMI, the word "tag" refers to data tags in the Logix controller.
Function
The IND570 EtherNet/IP interface kit enables the IND570 terminal to communicate to EtherNet/IP Programmable Logic Controllers (PLCs) through a direct connection to the EtherNet/IP network at either 10 or 100 MBPS speed. The kit consists of a backplane-compatible I/O module, mounting hardware, and a ferrite. Various types of data exchange to allow reading and writing of different weighing and control parameters for the IND570 terminal is available. Configuration to setup the type of data exchange resides in the IND570 terminal.
Features
- User programmable IP address, Subnet Mask and Gateway address.
- Unicast I/O for EtherNet/IP allows for direct point-to-point communication between two devices on a network. This communication format is more efficient when I/O data does not need to be shared between multiple target devices.
- Capability for bi-directional discrete mode communications (Class 1 Cyclic Messaging) of weight or display increments (in integer or floating point format), status, and control data between the PLC and the IND570.
- Support for Explicit Messaging to access IND570 shared data variables.
- Offers specific data integrity bits to allow the PLC to confirm that data exchange is valid.
- There may be up to 4 message slots for discrete data transfer, Class 1 messaging.
- Status LEDs to indicate communication, network and module status.
Network Connectors
Refer to manual for pinouts and Rockwell Automation part numbers of mating connector.
- The wiring between the PLC and the IND570 EtherNet/IP Interface kit uses a standard ethernet twisted pair cable with a RJ-45 connection. Cables are not supplied by Mettler-Toledo.
- The cable installation procedures and specification including distance and termination requirements are the same as recommended by Allen-Bradley for the EtherNet/IP network.
Module Identity
The module Identity includes the following Device attributes:
- Vendor ID '666', and Vendor Name string 'Mettler-Toledo'
- Product Type '12', and Product Type Name string 'Communications Adaptor'
- Product Code '11', and Product Name string 'IND570-ETHIP'
- Catalog Name string 'IND570-EtherNet_IP'
Communications
The IND570 EtherNet/IP Interface uses EtherNet/IP Implicit communication for transferring I/O data to a controller. Certain data can also be accessed using EtherNet/IP explicit messaging. CIP messages are supported from a host device over the EtherNet/IP network.
Note
: Refer to the manual for full details of these communication protocols.Input and Output Tag Data
The following module Input and Output tags are created in the RSLogix5000 project by the AOP.
Note
: Logix IO tags are updated by the controller asynchronous to its ladder-logic program scan. When "block integrity" of this data is important, the CPS ladder instruction can synchronously copy the data to other Logix tags for use by application logic. Note
: Default RPI
for the IO connection is 25ms
. It is important to set the Requested Packet Interval for an update time suitable for the application. The update time chosen determines how often the host will receive Input Image updates from the IND570 EtherNet/IP Interface. A very long RPI will result in events taking place at the IND570 EtherNet/IP Interface module that may never be seen by the host logic.Integer or Division Data Format
The Integer data format reports the weight data with an integer value in the current weight units and Division reports the data with a weight value in the number of divisions (scale increments). When one of these formats is selected in the IND570 setup configuration, the IND570 will have two 16-bit words for input data and two 16-bit words for output data in each Message Slot. Up to 4 message slots are available and each can be assigned for a specific scale channel's data. (The comparator status bits are only available with IND570 software 5.0 or greater.)
Below is the view of an IND570 device
Integer/Division Input Tag
with 2 message slots, with the second slot expanded to show the two words, Weight and Status. The 1st word of the message slot, Weight, is a 16-bit signed integer of the scale weight value in weight units or divisions. The second word of slot 2, Status, consists of status bits to indicate scale and I/O statuses. The second word is expanded to show the tag names of the individual bits. Note
: Decimal bit numbers are shown in the Description column (which is added by the user). Octal bit numbers can also be used in the IND570 Terminal. Refer to the IND570 Terminal PLC Interface Manual for more details on the data definitions.
RSLogix5000 View of Integer/Division Input Tags - 2 message slots (description added by user)

Below is the view of an IND570 device
Integer/Division Output Tag
with 2 message slots, with the second slot expanded to show the two words, Weight and Command. The 1st word of the message slot, Weight, is a 16-bit signed integer of the weight value in weight units or divisions, that is for download to the IND570 as a tare or target value. The second word of slot 2, Command, consists of command bits to trigger a write of the 1st word output value to the IND570, and to trigger scale functions and set I/O in the IND570. The second word is expanded to show the tag names of the individual bits. Note
: Decimal bit numbers are shown in the Description column (which is added by the user). Octal bit numbers can also be used in the IND570 Terminal. Refer to the IND570 Terminal PLC Interface Manual for more details on the data definitions.
RSLogix5000 View of Integer/Division Output Tags - 2 message slots (description added by user)

Floating Point Data Format
The floating-point data format reports the weight data with numeric data encoded in IEEE 754, single precision floating point format. The floating point format provides four 16-bit words of input data and three 16-bit words of output data per Message Slot. Up to 4 message slots are available and each can be assigned for a specific scale channel's data.
Below is the view of an IND570 device
Floating Point Input Tag
with 3 message slots, with the third slot expanded to show the four words, Command Response, Data1, Data2, and Status. The high byte of the 1st word of the message slot, CMD_Response, includes bits to indicate the type of data that is being sent in the floating point input words and the command acknowledgement status bits. This SINT is expanded to show the bit tag names. The low byte of this word is reserved and not shown in the display. The 2nd and 3rd words, FPdata1 and FPdata2, together represent the 32-bit single precision floating point value of the scale data that has been requested with the Discrete Write command. The 4th word, Status, consists of status bits to indicate scale and I/O statuses, and is expanded below to show the bit tag names. Note
: Decimal bit numbers are shown in the Description column (which is added by the user). Octal bit numbers can also be used in the IND570 Terminal. Refer to the IND570 Terminal PLC Interface Manual for more details on the data definitions.
RSLogix5000 View of Floating Point Input Tags - 3 slot example (decimal bit number)

Below is the view of an IND570 device
Floating Point Output Tag
with 3 message slots, with each slot expanded to show the three words, Command, FPData1, and FPData2. The 1st word of the message slot, Command, is used to instruct the IND570 on what data to send for the Discrete Read data, to write the floating point load word value into the IND570, and to trigger scale functions and I/O. The 2nd and 3rd words, FPLoadData1 and FPLoadData2, together represent the 32-bit floating point load word value that is to be sent to the IND570.Note: Refer to the IND570 Terminal PLC Interface Manual for more details on the command definitions.
RSLogix5000 View of Floating Point Output Tags - 3 slot example (decimal bit number)

Provide Feedback