Documentation

Manual
The primary source for detailed information about this module is the "IND570 Terminal PLC Interface Manual", available from the IND570 Documentation CD (P/N # 30205330) included with the terminal.
EDS File
The EDS file is used for identifying the module to network tools, such as RSNetWorx or a CIP (refer to "CIP" in RSLogix5000 HELP) network browser (e.g. RSLinx Who). The EDS file can be retrieved from the IND570 Documentation CD (P/N # 30205330) and installed using the RSLinx Hardware Installation Tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal