Indicators and LEDs
The ACT350 EtherNet/IP Interface which is located inside the ACT350. Note that there is a serial port on the top of the unit where tools such as the
Setup+™
Configuration Tool can be connected.
Provide Feedback