Troubleshooting
Module Indicators/LEDs
Refer to the section Indicators and LEDs.
RSLogix5000 Diagnostics
RSLogix5000 software indicates module fault conditions in the following three ways:
- Warning signal on the main screen next to the module, when the IO connection is broken
- Fault message in a screen's status line, with notification in the Tag Editor. General module faults are also reported in the Tag Editor. Diagnostic faults are only reported in the Tag Editor.
- Status on the Module Info Page
Provide Feedback