Totalizers
Assign Process Variable to Totalizer
Select process variable for totalizer
TIP:
If the option selected is changed, the device resets
the totalizer to 0.
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Volume flow |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Totalizer Unit
Select process variable totalizer unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | l |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Totalizer Operation Mode
Select totalizer calculation mode
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Net flow total |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Totalizer Preset Value
Specify start value for totalizer.
Property | Value |
|---|---|
Selection / Range | -3.4E+38 - 3.4E+38 l |
Factory Setting | 0 l |
Visibility | Operator |
Write Access | Operator |
Data Type | FLOAT |
Totalizer Failure Mode
Specify how the totalizer should behave in the event of a device alarm.
TIP:
The failsafe mode that applies to any other totalizers
or outputs is specified separately in other parameters and is not impacted by this setting.
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Stop |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Totalizer Control
Operate the totalizer.
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Totalize |
Visibility | Operator |
Write Access | Operator |
Data Type | ENUM16 |
Provide Feedback