Process Parameters

Filter Options

Select filter option to adapt the output signal to the application
Filter Options parameter properties
Property
Value
Selection / Range
  • Adaptive
  • Adaptive CIP on
  • Dynamic
  • Dynamic CIP on
  • Binomial
  • Binomial CIP on
Factory Setting
Binomial
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Flow Damping

Enter value for damping of the flow measured value in order to reduce the variability of the flow measured value when exposed to interference.
The depth of the flow filter is determined by this setting. As the filter depth increases, so does the reaction time of the device.
  • Value = 0: No damping. Damping of 0 is not recommended, as the measuring signal is so noisy that it is almost impossible to perform a measurement.
  • Value > 0: Damping increases
Optimal damping depends on the measuring period.
Damping impacts the following measuring device variables:
  • Outputs
  • Low flow cut off
  • Totalizers
Flow Damping parameter properties
Property
Value
Selection / Range
0 - 15
Factory Setting
4
Visibility
Operator
Write Access
Maintenance
Data Type
UINT8

Flow Override

Stops the measuring process. Can be used for example when cleaning the pipeline.
When flow override is activated the diagnostic message "453 Flow override active" is generated.
Output values when flow override is activated:
  • Temperature: Measurement continues
  • Totalizers 1 to 3: No longer totalize
Flow Override parameter properties
Property
Value
Selection / Range
  • Off
  • On
Factory Setting
Off
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Conductivity Measurement

Switch conductivity measurement on or off.
TIP: To be able to measure conductivity, the medium must have a minimum conductivity of 5 μS/cm.
Conductivity Measurement parameter properties
Property
Value
Selection / Range
  • Off
  • On
Factory Setting
Off
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Conductivity Damping

Enter value for damping the conductivity value
Conductivity Damping parameter properties
Property
Value
Selection / Range
0 - 999.9 s
Factory Setting
0 s
Visibility
Operator
Write Access
Maintenance
Data Type
FLOAT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal