Low Flow Cut Off
Assign Process Variable
Select process variable to activate low flow cut off.
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Volume flow |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
On Value Low Flow Cutoff
Enter value to switch on low flow cut off.
Value = 0: No low flow cut off
Value > 0: Low flow cut off is activated
Property | Value |
|---|---|
Selection / Range | >= 0 |
Factory Setting | 0 l/h |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Off Value Low Flow Cutoff
Enter value to switch off low flow cut off.
The off value is entered as a positive hysteresis with respect to the on value.
Property | Value |
|---|---|
Selection / Range | 0 - 100.0 % |
Factory Setting | 50 % |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Pressure Shock Suppression
Enter time frame for signal suppression (= pressure shock suppression active), for example
to prevent the device from registering flow movements in the pipe when a valve is
closed.
Pressure schock suppression is activated when the flow rate drops below the on value for
low flow cutoff.
Output values when pressure shock suppression is active:
- Flow: 0
- Totalizer: Last valid value
Pressure shock suppression is deactivated when the time frame specified has elapsed and
Flow exceeds the off value for low cutoff
Property | Value |
|---|---|
Selection / Range | 0 - 100 s |
Factory Setting | 0 s |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Provide Feedback