External Compensation
Density Source
Select source of the density for the density compensation
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Fixed density |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Fixed Density
Enter a fixed value for the density.
TIP:
The applicable unit of measure is specified in the
"System units" submenu
Property | Value |
|---|---|
Selection / Range | 0 - 3.0e+38 kg/l |
Factory Setting | 1000 kg/l |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Temperature Source
Select source of the temperature for the temperature compensation
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Off |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Provide Feedback