Custom Input Connection
Input Assembly Positions 1-10
Assignment of process variable to positions 1-10 of the custom input data.
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Volume flow |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Input Assembly Positions 11-15
Assignment of process variable to positions 11-15 of the custom input data.
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Actual diagnostics |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Provide Feedback