Build-Up Detection

Build-Up Index

Select mode for build-up index.
The interval for determining the build-up measured value can be specified here.
  • If experience shows that build-up forms quickly, then a fast interval should be selected. Also for cleaning cycles.
  • If build-up forms over months, then a slow or standard interval is sufficient.
Measurement every:
  • Slow: 600 sec.
  • Standard: 60 sec.
  • Fast: 6 sec
TIP: The build-up index is only available in conjunction with Heartbeat Technology. If Heartbeat Technology was ordered together with the measuring device, the option will already be enabled, and no further action is required. If Heartbeat Technology was ordered at a later date, you must first activate the option under "Activate SW option" by entering the activation key you received. To purchase Heartbeat Technology, contact your local sales and service center. In addition to Heartbeat Technology, conductivity measurement must be enabled on the device. To do this, go to the "Conductivity measurement" parameter on the "Process parameters" menu and select the "On" option.
Build-Up Index parameter properties
Property
Value
Selection / Range
  • Off
  • Slow
  • Standard
  • Fast
Factory Setting
Off
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Build-Up Index Damping

Enter damping value for build-up index
TIP: The build-up index is only available in conjunction with Heartbeat Technology. If Heartbeat Technology was ordered together with the measuring device, the option will already be enabled, and no further action is required. If Heartbeat Technology was ordered at a later date, you must first activate the option under "Activate SW option" by entering the activation key you received. To purchase Heartbeat Technology, contact your local sales and service center. In addition to Heartbeat Technology, conductivity measurement must be enabled on the device. To do this, go to the "Conductivity measurement" parameter on the "Process parameters" menu and select the "On" option.
Build-Up Index Damping parameter properties
Property
Value
Selection / Range
0 - 15
Factory Setting
0
Visibility
Operator
Write Access
Operator
Data Type
UINT8

Build-Up Index Value

Shows current build-up index value
TIP: The build-up index is only available in conjunction with Heartbeat Technology. If Heartbeat Technology was ordered together with the measuring device, the option will already be enabled, and no further action is required. If Heartbeat Technology was ordered at a later date, you must first activate the option under "Activate SW option" by entering the activation key you received. To purchase Heartbeat Technology, contact your local sales and service center. In addition to Heartbeat Technology, conductivity measurement must be enabled on the device. To do this, go to the "Conductivity measurement" parameter on the "Process parameters" menu and select the "On" option.
Build-Up Index Value parameter properties
Property
Value
Selection / Range
0.0 - 3.4E+38 %
Factory Setting
0.0 %
Visibility
Operator
Write Access
Read-Only
Data Type
FLOAT

Build-Up Limit

Enter limit value for the build-up index
TIP: The build-up index is only available in conjunction with Heartbeat Technology. If Heartbeat Technology was ordered together with the measuring device, the option will already be enabled, and no further action is required. If Heartbeat Technology was ordered at a later date, you must first activate the option under "Activate SW option" by entering the activation key you received. To purchase Heartbeat Technology, contact your local sales and service center. In addition to Heartbeat Technology, conductivity measurement must be enabled on the device. To do this, go to the "Conductivity measurement" parameter on the "Process parameters" menu and select the "On" option.
Build-Up Limit parameter properties
Property
Value
Selection / Range
0 - 100 %
Factory Setting
50 %
Visibility
Operator
Write Access
Operator
Data Type
FLOAT

Build-Up Limit Hysteresis

Enter hysteresis for build-up limit value
TIP: The build-up index is only available in conjunction with Heartbeat Technology. If Heartbeat Technology was ordered together with the measuring device, the option will already be enabled, and no further action is required. If Heartbeat Technology was ordered at a later date, you must first activate the option under "Activate SW option" by entering the activation key you received. To purchase Heartbeat Technology, contact your local sales and service center. In addition to Heartbeat Technology, conductivity measurement must be enabled on the device. To do this, go to the "Conductivity measurement" parameter on the "Process parameters" menu and select the "On" option.
Build-Up Limit Hysteresis parameter properties
Property
Value
Selection / Range
0 - 100 %
Factory Setting
20 %
Visibility
Operator
Write Access
Operator
Data Type
FLOAT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal