Access Rights

Access Status

Displays the role the user is currently logged on in. The role determines the users access rights for the parameters.
TIP: Until a Maintenance code has been set in the "Define Maintenance code" parameter, all users are automatically logged on in the Maintenance role. Once the Maintenance code has been set, all users are automatically logged on in the Operator role.
TIP: The access rights can be changed via the "Enter access code" parameter.
Access Status parameter properties
Property
Value
Selection / Range
  • Operator
    Provides only read access to parameters.
  • Maintenance
    Provides read and write access to parameters.
    For some parameters, the user must be logged on in the Service role to obtain write access.
  • Service
  • Production
  • Development
Factory Setting
Maintenance
Visibility
Operator
Write Access
Read-Only
Data Type
ENUM16

Enter Access Code

For users logged on in the Operator role, enter the Maintenance code to change the access status to Maintenance and disable write protection of parameters. For users logged on in the Maintenance role, enter the Service code to change the access status to Service and enable read and write access to Service parameters.
Enter Access Code parameter properties
Property
Value
Selection / Range
0 - 9999
Factory Setting
0
Visibility
Operator
Write Access
Operator
Data Type
UINT16

Write Protection

Write Protection parameter properties
Property
Value
Selection / Range
  • Off
  • On
Factory Setting
Off
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM8
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal