Sensor Adjustment

Installation Direction

Set sign of flow direction to match the direction of the arrow on the sensor
Installation Direction parameter properties
Property
Value
Selection / Range
  • Flow in arrow direction
  • Flow against arrow direction
Factory Setting
Flow in arrow direction
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal