Documentation

Manual

The primary source for detailed information about this module is the Endress+Hauser document, “Promag 300/500 EtherNet/IP Supplementary Documentation”, available for download from the Endress+Hauser website (www.endress.com).

EDS File

The EDS file is used for identifying the module in network tools, such as RSNetWorx or in CIP (refer to “CIP” in RSLogix 5000 HELP) network browser (e.g. RSLinx Who). The EDS file can be downloaded from the “Endress+Hauser website” and installed using the RSLinx Hardware Installation Tool.

Certifications

Certifications for this module normally include CE. Refer to the markings on the transmitter nameplate and to the specifications in the Promag 300/500 Operating Instructions for more detailed information. Products with a CE mark are approved for installation within the European Union and EEA regions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal