Process Parameters

Conductivity Damping

Conductivity Damping parameter properties
Property
Value
Selection / Range
0 - 999.9 s
Factory Setting
0 s
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
FLOAT

Flow Override

Flow Override parameter properties
Property
Value
Selection / Range
  • Off
  • On
Factory Setting
Off
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Filter Options

Filter Options parameter properties
Property
Value
Selection / Range
  • Adaptive
  • Adaptive CIP on
  • Dynamic
  • Dynamic CIP on
  • Binomial
  • Binomial CIP on
Factory Setting
Binomial
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Flow Damping

Flow Damping parameter properties
Property
Value
Selection / Range
0 - 15
Factory Setting
4
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
UINT8
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal